By a circuit using TPS40192, undershoot occurs to an output voltage wave pattern the output side
in Vdd side power supply Off in no load, and negative electric potential may occur at one time.
It drives Low side Gate to ON then.
I want you to teach a probable cause, because I investigate the logic of the outbreak.
Condition:
a. The normal is Vdd=12V,Vo=1V
b. The output side to be in an electric discharge state, and to overcome that the input voltage is slow
in stop voltage neighborhood (Vdd=about 3.5V) of the IC is no load.
c. The drop time of Vdd more than 200mS/V.
Other information:
a. It does not occur by all means.
b. The switching wave pattern of the Gate drive stops once on the way and drives Low side Gate
to ON after about 7.5mS.
c. In this time, I do not seem to influence it at descent time of Vdd.
d. The step of the middle electric potential of the COMP wave pattern lasts time of about 900μS.
e. The middle electric potential of the COMP wave pattern is about 240mV.
f. When Low side Gate becomes ON, COMP signal stands up by a chopping wave from 0V and falls into Low
when it became around 400mV.
g. The chopping wave start of the COMP signal is time of about 330μS to the voltage of around 400mV.
h. It is time of the about 1.2mS until it drives Low side Gate to the chopping wave start of
the COMP signal from the beginning.
i. Even if there is the resistance equal to 100kΩ between SW-BOOT listed with EVM board,
it occurs even if there is not it.
j. The oscillatory frequency of TPS40192 is approximately 610kHz.
Thanks,
Masami