This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Adjustable output DC-DC power supply design

Dear All,

I am looking into design a DC-DC buck power supply with below features. I am trying to implement it with DC-DC buck converter with DAC feedback on FB pin to achieve output adjustment.

1) 15 - 24v DC input

2) Adjustable output from 1V - 14.5V, resolution depends on DAC resolution

3) Continues 4A driving capability, with 6A peak for few seconds

4) Adjustable power up/down slow rate as fast as 100 uS, with 100 uS step size (So that slow rate can be achievable in a wide range For example, 100uS, 200uS, 300uS .... 1mS..20mS.......5S ......10S) 

I can use micro-controller to contol DAC to do power margin adjustment. But for fast slow rate, I am not sure which components can achieve this. Is there anybody can recommend me suitable DC-DC converter and DAC can achieve above design spec. Thanks.