Dear FAE,
I would like to send complete design details and test data.
Please respond to htaylor@comverge.com
Best Regards,
Harold Taylor
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear FAE,
I would like to send complete design details and test data.
Please respond to htaylor@comverge.com
Best Regards,
Harold Taylor
Hi Harold,
You can either post the data here or email us at SimpleSwitcherApps@ti.com.
Best Regards,
-Juan
Bringing up the post for Harold. He is still waiting for assistance with this issue.
Hello,
I am suspicious that the LMP8646 may contribute to this problem. The ripple current can be higher during start-up, and if the LMP8646 detects a current limit during start-up then in may get stuck in that mode. Can you remove R155 to remove the LMP8646 from the circuit and repeat?
Regards,
Mike
I have tried reducing the output inductor value and this eliminates the oscillation problem into full load. However, the output switching noise is much higher (on the order of 400 mV p-p with Lout = 2.2 uH where the original value was <100 mV p-p with Lout = 4.7 uH). Also, I have not seen significant reduction in the amount of transient droop when I reduce the Lout value and increase the Cout value.
I will try removing R155 to determine if the LMP8646 is contributing to both issues.
I removed R155 (steering resistor for the LMP8646) and the startup oscillation still persists with my initial values. Increasing the output capacitance appears to kill the oscillation, but I need to re-try this experiment with all ceramic caps (used a ceramic-electrolytic-parallel combo last night). I will perform additional experiments today.
HT