1)The noise performance is for VDO >= 1V.
Please check if they have any info on noise degradation Vs VDO.
i.e. : is noise performance degrade for VDO = 0.3V
2) Is it no need for Cff parallel to R1 ?.
.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Noise will vary very little as device operation approaches dropout. However, PSRR will be affected is the load current is such that the device is actually operating in drop-out mode.
Cff (across R1) is not required, nor recommended. Cff is typically used to add phase margin to an output power stage feedback loop with capacitive loading, In this case, R1 and R2 are used to set the DC reference voltage which is isolated from the output power stage by the low pass filter.