I am using the TPS65910A1 to power the Sitara AM335X.
What is the VBACKUP voltage limits (min, max) specifications for this IC?
Currently the design is using a Lithium Ion rechargeable battery connecting to the VBACKUP terminal of the TPS65910. This is used to support the RTC functionality. This series battery when fully charged is a 3.0 Voltage source. I am interested in switching to a higher capacity lithium battery having a nominal Voltage of 3.6V.
The nearest parameter in the SWCS046N –MARCH 2010–REVISED APRIL 2012 datasheet for VBACKUP I can find is VRTC_LDO when in BACKUP, which is specified at 1.9V min and 3.0V max. I would find it difficult to believe this applies to VBACKIP since the max voltage of lithium ion battery as used on the reference design is at the limits without margin.
So, what is the VBACKUP Voltage range?
Thanks,