Hello,
I my design I am planning to use up to 16 TLC5927 daisy chained, but I have some questions regarding such implementation:
1) Which is the capacitance each TLC5927 pin represents? I am worried that the clock, OE and LE signals of the MCU cannot drive the total capacitance represented by all 16 TLC's plus the PCB traces.
2) Does the TLC communication lines need a external pull up or the TLC has internal pull ups? In case a external one is needed, Which value is the most adequate? As you can see I will have 4 groups of 4 TLC's each, the distance between the SDO of one group to the SDI line of the next group can have a distance of 600mm (I think this distance can be the worst case scenario).
Attached is a small diagram showing the MCU-TLC interconnection, the problem here is that I do not know the exact trace length (the number shown is an approximation)
Best regards
Mark