Other Parts Discussed in Thread: BQ24073, BQ24250, BQ24072, BQ24392
Hi Guys,
Currently I'm using BQ24073 IC for my battery charging, I fixed it to USB500, however, I'm thinking if this is possible to set dynamically (input current) from setting this to USB500 to 1A depends on the charger capability.
I want to set them from USB500 to 1A input current using a Power supply charger dynamically. First test if it is connected to USB.
The problem is that it should sense if it is connected to USB or is it just a power supply.
Im open also to change my design if there is a better IC out there.
Your advise is highly appreciated or if you experience same challenge before.
Thanks and regards,
Jay