This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40054 Maximum duty cycle too low

Other Parts Discussed in Thread: TPS40054

I want to charge a battery to 14V from a solar panel which has it's max. power point at around 15.5V.

Is there a way to increase the maximum duty cycle above the worst case value of 85% at an input voltage of 15.5V?