hi,
i am looking for a buck switching regulator having following specifications,
input voiltage range 4-60 Volts
output voltage 5 volts
output current 1A
Main requirement : the start-up time should be less than 20usec
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi,
i am looking for a buck switching regulator having following specifications,
input voiltage range 4-60 Volts
output voltage 5 volts
output current 1A
Main requirement : the start-up time should be less than 20usec
How much output capacitance would you need in this application? With this start up time it may be the main limiting factor. For example if 47uF were used, the amount of current needed to charge up the output capacitor would be I = C dV/dt = 47uF * 5V/20us = 11.75A. I do not have a good recommendation yet but this is making me think to use a device with a higher current limit than is required for the nominal 1A output.