For the TL7733B supply voltage supervisor, it is apparent from the datasheet that the recommended operating supply (VCC) voltage is 3.6 to 18 V.
However, the application information Figure 8 (of the datasheet) shows an example where the system supply (VCC) is the same voltage being monitored at the SENSE input.
If the system supply is 3.3 V, does this imply that the 3.3V supervisor cannot be used in the configuration of Figure 8 since 3.3 V is below the recommended operating voltage?
If so, how might the IC be used to monitor 3.3V?
Is there a reference design where the TL773B is used to monitor 3.3V?