I have designed one power supply using UCC28019 PFC controller followed by UCC28600 Quasi resonant converter but audible noise is coming from my power supply My input and output specifications as follows
Input voltage- 115V ac
input frequency- 360Hz to 800Hz
My PFC stage will convert this to 250V dc and then quasi will convert 250V to 12V/ 60W. I used my own inductor for the PFC stage. Is that Audible sound is due to my inductor or My input input frequency?. Even no load also sound is coming. Is there any problem for using that controller in 360Hz to 800Hz frequency range? Can anybody suggest How to eliminate that noise?