This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC1524A Performance with Load Outside of Range on Datasheet

Other Parts Discussed in Thread: UC1524A

Hello,

We I am currently using the UC1524A in a circuit and am experiencing some issues with its output performance from pin 9.

The datasheet uses a load range from 30k to 1Meg ohms. Due to control loop requirements, we are using a resister value of 499 ohms. This causes what looks to be current limiting from the error amp within the IC.

Is there any more information on the current sourcing capabilities of this error amp? The datasheet mentions a maximum "forced" current from pin 9 to be +- 10mA but I am not entirely certain that this is what I am looking for.