Hi,
I recently acquired bq500211AEVM-210 and BQ51013BEVM-764 but they doesn't seem to be working.
I've connected the transmitter to a DC-source that supplies 5V and around 35mA to the transmitter and diode D1 glows.
TP1 is connected to an oscilloscope, which shows the pulses that are described in the user guide.
The receiver is connected via J3 and J4 to a variable resistor set to 5 Ohms.
I place the receiver on top of the transmitter and make sure the coils are aligned, then I wait for something to happen but nothing happens.
I check TP1 and it's still giving of the same pulses as without receiver.
I do some measurements on the receiver at TP2 and TP4 and they confirm that the transmitter is sending pulses.
There's no output power from the receiver and only diode D1 glows on the transmitter, all the other diodes on the receiver and transmitter are dark.
The transmitter continues to draw the same amount of power as before (5V, 35mA).
I've checked the settings on the receiver before I started testing and they are correct.
The jumpers are set according to datasheet, and I've measured the resistors R3 and R16 and they are set to the right value according to the datasheet.
I've tested the variable resistor and it's working and it can handle the power that the receiver can output.
I don't know what else I can do, everything indicates that the "handshake" between the units fail but I can't find what's wrong.