Please tell me the Min and Max value of the following reading parameters.
-Temperature
-Voltage
-Current
-Cell Voltage[1:4]
In the datasheet, each parameter register has Min and Max value.
ex) Voltage: Min 0, Max 65535
If Voltage register value is 60000, is 60000 returned by read command?
Or does firmware have lower and upper limit?
If firmware doesn't have limit, does EVSW have limit value?