Hi ,
I am trying to se the LBO pin on the TPS61092. In my circuit I have the LBO connected to the gate of a PNP transistor (through a 270 ohm series resistor). When my LBI reaches it's threshold voltage (greater than 500mV) nothing happens on the LBO. I do have a 1M pull up on the output of the LBO (tied to V out). I know it should be pretty straight forward but I am missing the obvious. I have tried two other boards and they exhibit the same behavior.
Thanks for any input