This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Current Fed Full-Bridge Isolated Boost Converter / Current Fed Step Up

Other Parts Discussed in Thread: LM5045, UCC3895, TL494, UC28023, UC28025, LM5046, LM5041B

Hi Ti

I'm about to design a current fed full-bridge converter

Specs:
Vin: 27V - 42V
Iin: 13A
Vout: 300V - 600V 

What i need is a pwm controller  that is able to go above 50% duty cycle on all switches.

The schematic is as follows.

I have looked at the LM5045, would this IC be suitable?

I'm curious as there is no description of a inductor on the input side, or mentioning of duty cycles above 50%.

If there is a more suitable IC, i would be happy to know.

Best regards
Kristian K