I have a design using the TPS55010, running at 107KHz, about 42% duty cycle, using transformer Coilcraft p/n JA4650-BL (primaries in series, secondaries in series).
Load current is 8.5mA max nominal, output 6V, input 5V.
All parts selected using TI's single output spreadsheet. I've also tried running up to 350KHz (various component values adjusted, of course).
Load current is 8.5mA max nominal.
I am getting about 76% efficiency, tops (input current ~14mA). I need to squeeze out 90-91% if I can (input current of 11.25mA max). What should I vary to get this? Reduce duty cycle (increase turns ratio)? Or reduce/increase transformer primary inductance? Some other?
Thanks,