Hello,
I am creating an isolated full bridge DC/DC converter using the UCC28950. It will have a large input voltage range of 300V-650V. My question is how to power the UCC28950 itself. I am thinking one option is to design a small wide-input flyback converter to power the UCC28950 and the gate drivers. I also saw the PMP5410 design example which shows the UCC28950 powered from a non-isolated buck regulator. However, the feedback must be opto-isolated. It seems like the main difference is whether the UCC28950 is referenced to the input or the output. I am wondering which method is better? My biggest concern is size and weight. Cost is not the biggest concern. Thanks for any help!