Hi,
Our customer considers to use LM5642.
Please let me know about LM5642.
Please let me know about LM5642.
Can I use LM5642 with single output?
Are following pin connections for single output correct?
・ON/SS2(10pin)→GND
・Vdo2(19pin)→open
・COMP2(12pin)→open
・ILIM2(13pin)→open
・KS2(14pin)→open
・RSNS2(15pin)→open
・HDRV2(17pin)→open
・CBOOT2(18pin)→open
・SW2(16pin)→open
・LDRV22(20pin)→open
・FB2(11pin)→open
LM5642 is used in the existing system.
so customer want to use it.
best regards,
Yusuke