This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PTH08T250W, 3 in parallel, DAC to margin, heat removal

Other Parts Discussed in Thread: PTH08T250W

Gentlemen,

I have three questions on the PTH08T250W.

I would like to put three in parallel and cannot find that this is ok. All examples are only for two in parallel and there is never any mention that more than two can be put in parallel. I have additionally referenced the application note “ Paralleling power modules for high-current applications” that did not address this issue.

Is it possible to trim or margin the power supply using a DAC instead of a resistor between pins 4 and 18?

Using the supply for high current what parts do I need to remove heat from if there is little or no air flow?

Thanks,

-tom