Is there any errata on the tlv62090? We have a customer that is having a problem when there is no SS capacitance the regulator won’t start at Vin = 5.0V. They are also having a problem starting with 6800pf at 85C and Vin = 5.0V on some parts.
Vin range is 3.3 to 5.5 the problem is Vin > 4V
Vout is 1.0V
The load current while running is .5A to 1A
The current should be the same + or – 10% due to temperature difference. They don't see the problem when they added 10,000pf to the 6800pf SS cap.
See attached schematic.