This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28051 output current drift

Hi     everyone.

My customer   used  UCC28051DR.

I  want   check  the  output current drift  this view.

  <conditions>

        ① MUL-pin ; 0.2V FIX

   ② Vo_sns ; 2V FIX

   ③ Current sensing-Register ; Rcs; 1/3Ω

   ④ output current deta waveform ; Zerocrosstalk

◆View

 ① Vcs=0.67×(Comp-2.5)×(MUL+0.075)

   Io=1/2×(Vcs/Rcs)

   Engeer think output drift current 560~840mA range?

   that using ucc’neighboor comp is 4.5~5.5V range,  and fix  range MUL , CS,  Vo_sns.

 

 ② Can you controls current output method a Volume Resister to MUL?

 

 ③ comp drift=output drift

   Is it eases high output capabilly COMP  to  the  supply capabilly REF-voltagecomp’s output capabilly include?

 

   from  Ben.

  • The multiplier gain constant (K) is a tested parameter and can be found on page 4 of the data sheet.  This parameter is specified from 0.43 to 0.87 with a typical of 0.65.  With this information the multiplier output voltage could vary +34% to -31% roughly.  However based on the output power the voltage loop will correct for errors in the multiplier and this is generally not an issue in the typical application.

    Regards,

  • Hi MIke.

    Thank you for reply.    It was very helpful.

    Sorry . Question No3 that I write was not good.

    Once again NO3.

    ③ Comp drift has given Vout drift.

      in this case.

      Comp output spec < REF-voltage good capabilly output

      Can be stop the Vout’drift include the REF?

     

    Regard.     from Ben

       

     

     

  •  

    The comp voltage should be adjusted by the voltage amplifier feedback to control the output voltage.  I am surprised that this is drifting.  How much is the drift and under what test conditions?

    Regards,

  • Hi   Mike.

    Thank you  for  returns.

    I  check for customer  that   the reply got from Mike.

    If let me consult for my customer 's  relation between comp drift and ref-voltage.

    Regards              from   Ben