I search in datasheet of BQ2205 and I don't found the max output current from Vout pin. I see only information about Vcc supply current Typ:210uA to max:500uA. I need Max current output of VOUT pin from VCC pin and BCp pin.
Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I search in datasheet of BQ2205 and I don't found the max output current from Vout pin. I see only information about Vcc supply current Typ:210uA to max:500uA. I need Max current output of VOUT pin from VCC pin and BCp pin.
Thank you!
Hi Tommy,
For this device, it is recommended not to exceed 80mA on VOUT as shown under the test conditions in the electrical characteristics table of the datasheet. Typical 3V standard low-power CMOS SRAM applications require around 20mA or less depending on speed. Therefore, 80mA is more than enough to power multiple banks of CMOS SRAM as shown in the datasheet's application diagram.
Regards,
Darwin