This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Electromagnet power supply

Other Parts Discussed in Thread: LM5118

Hi,

I have a requirement of supplying varying voltages from an incoming 24V DC source to an electromagnet. I need to derive 40V from 24V with about 2A output current requirment and dynamically change the output voltage from 40V to 12V in steps. Is there any I2C/SPI controllable buck-boost regulator? If not, is there a buck-boost converter whose feedback voltage can be changed using a DAC to change the output voltage from 40V to 12V in some discrete steps?

Regards,

Viswa