Hello, I am trying to find a flyback transformer that can be regulated to 600vdc; any help will be greatly appreciated.
Thank You
Anthony
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, I am trying to find a flyback transformer that can be regulated to 600vdc; any help will be greatly appreciated.
Thank You
Anthony
Tell more about your project and I will be here!
I am charging a 600VDC capacitor bank but do not want\need the excess voltage produced by the flyback. It has been several years since I worked with flybacks.
Thank You
Anthony
Input will be 12VDC from a car battery
peak-power 3amps X 600V = 1800W
preffered frequency 15Khz should work
first of all this not the power for flyback topology. the best option is a full bridge.
second 1800W/0.9/12=166A and the battery capacity must be >100Ah to hold the voltage under the load. (0.9=efficiency)
third 15khz is out of date now,f>30khz is fine.