This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq34z100 VEN input high level threshold

I think high level input is needed to VEN pin for detection of push button ON.

So, I want to know the high level threshold. 

Please let me know that information.

And I have one more question.

In datasheet circuit, there is 1k ohm resistor betwenn VEN and REG25.

Is it no problem that this resistor is modified to 500 ohm?