Hello,
I have a customer that is trying to find a way to have the following parameters:
Vout: 3V - 15V
Vin: 6V - 9V
Iout: 2.25A
It looks like the LM5118 or LM25118 could work based on the described allowable ranges in the datasheet. However, I would like to confirm this since we are using Vout ranges both above and below the Vin range.
Can a configuration be done with this device to attain this output?