I am working on a DC motor control and I would like to know if the TL783 can be used. I need 90 Vdc at 10 amps maximum current. I see in the data sheet (Fig. 19 & 20) that the TL783 can be used as a shunt regulator with transistors to boost current. I have a Toshiba MG15H1AL1 IGBT transistor module rated at 600 V @ 150 A. that I would like to use as either a series losser element or shunt element. I have a power supply made with a 1100 watt transformer and a Toshiba 106L2C43A full wave rectifier rated at 600 V @ 160 A. I have a 3900 µF capacitor for a filter.
My no load voltage is 140 Vdc. With a 24 Ω load it drops to 123 Vdc @ 5.6 A with 10 Vpp ripple @ 120 Hz. This approximately the load my 1 HP DC motor would draw.