Dear TI,
1. Presently we are using TPS62090 regulator for our device. But now we need to change the regulator because we need to utilize the full battery voltage level even if reach till 3V. So we are choosing TPS63001 (If not, advice better one).
Device Requirement:
3.3V,1.2A
2. We need Battery charger IC,So please suggest the suitable IC for our requirement.
Requirement:
Li-Polymer Battery(2cells in parallel) 3.7V,20Ah.
Charging voltage for battery 4.2V,4Ah
input voltage for charger IC 5V
3. We need to display the remaining capacity of the battery like all mobiles do.And also we need to measure and display the battery temperature.So please suggest me the suitable IC for this application.