This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Combining PTEA404120 ICs for Increased Current?

Other Parts Discussed in Thread: PTEA404120

I am looking to see if TI can recommend an isolated power module that supports 20-70Vin and 12Vout @ 2A, 4A, and 6A. I have located the PTEA404120 which has a range of 36-75Vin and 50W output maximum (i.e. 4.2A max). Assuming that the 20V low input can be reasoned away for this design because the majority of telecom systems operate in the range of 36-72V, would there be a way to combine two of these PTEA404120 power modules in order to provide the desired maximum 6A output at 12V?

Thanks for your help!

Michael