Hello;
i am going to use tlc5971 in the design of a led screen. However i have some problems with the typical application circuits given in the datasheet. I intend to use the first application circuit in which internal linear regulator is used. My vcc is 12v and i will connect three leds in series per channel group and adjust the current as 40ma. The voltage across leds is 10,5v maximum for 40ma current. For this application, is the third app circuit in datasheet more suitable or not? in the third app circuit, should vled be exactly 15v? And i wonder why there are many leds in series in third app circuit whereas in the first app circuit there is only one led in datasheet figures?
My last question is if i use the first application circuit in datasheet, is it enough to use the given passive circuit components (capacitors,resistors) in application circuit or should i put some extra components to make the circuit more stable/rigid/goodWorking?
Thanks for your replies.