Can the TPS23753 support more than 13W output (@ 12V) to a device if a 12V DC adapter is used as described in SLVA306A Figure 8? If so, how much? I'm thinking the answer is no, 13W is the max due to the device being 802.3at Type 1 only.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can the TPS23753 support more than 13W output (@ 12V) to a device if a 12V DC adapter is used as described in SLVA306A Figure 8? If so, how much? I'm thinking the answer is no, 13W is the max due to the device being 802.3at Type 1 only.
The circuit in figure 8 bypasses the "POE" portion of TPS23753 and as such could be used with a dc/dc converter at > 13W.