This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS5450 Quiescent Current

Other Parts Discussed in Thread: TPS5450, TPS54531, TPS54540

I'm using a TPS5450 regulated in 5V (Vsense aprox 1,21V). In my tests the quiescent current with no load connected but with Vout ON and Vin=12V the consume is 0,2W. (17mA quiescent current). Looking in the datasheet there is no information about quiescent current while switching. Is there any way to calculate this value to check if I'm capturing the correct value.

Is there any guide for reducing the quiescent current? This value is critical for my project!

Thanks a lot!!