This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Testing BAT_LOW/BAT_GD of bq27510-g2

Other Parts Discussed in Thread: BQ27510

Hi,

I have to program and test our PCB with bq2710. My software programs it with a battery profile data, which seems to be done all right as our application software can display different charge levels of the battery on the screen.  But my test of bq27510 fails intermittently.  My method of testing bq27510 is as follows:

1. First we apply 4.5V to BAT, or pin 4.

2. Confirm that BAT_LOW/, or pin 12, is not active, or high.

3. Then we apply 2.4V to BAT.

4. Wait for 3sec.

5. Then we check BAT_LOW/ if it is active, or low. ----> THIS CHECK FAILS; bq27510 does not activate BAT_LOW/.

I am wondering if this test is valid for bq27510.  Any inputs will be appreciated.