Hi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Assaf,
The BQ25504 is capable of handling the load of the CC110L since it is typically under 40mA and the voltage range complies with the BQ25504.
Whether the solution can work consistently is dependent on the energy source that the BQ25504 is drawing the system and charging current from.