Dear Sir,
I am working on Bq-20z95 and want to use it with LCD instead of LED's for gas gauging.
I also want to use two Bq20z95 in series,so i have to connect Clock and Data in series.
can you insist me in this.
Regards
Tanvi Verma
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
I am working on Bq-20z95 and want to use it with LCD instead of LED's for gas gauging.
I also want to use two Bq20z95 in series,so i have to connect Clock and Data in series.
can you insist me in this.
Regards
Tanvi Verma
Dear Sir
Thanks for your reply. Is it is possible to Connect clock data in series.
Regards,
Tanvi
Tanvi,
I am not sure what you are asking about connecting the clock data in series. Could you please clarify?
Thanks
Tom
Dear Sir
i want to connect two Bq20z95 in a single circuit in series and on the same time i want Clock and data Communication from both PCB's at same Point. Is this possible ??
Regards
Tanvi Verma
Tanvi,
The device has SMBus address 16 hardcoded into its' SMBus controller, so it will only respond to that address per the SBS Specification. So, you will not be able to place two of the bq20z95 device on the same SMBus, because they would both try to process and respond to the same commands.
Regards
Tom
dear sir
thnx fo your reply
Sir can we use BQ20z95 in series without communication ????
The device can operate without the SMBus interface, but you will have to set the SLEEP bit low in the Operation Cfg A register to prevent it from going to sleep.