Hello,
TPS61500 will be operated at the moment even if EN is asserted Low when start up sequence.
Please see the attached file as sequence.
Please see the attached file as sequence.
In the datasheet Page5, there is below description.
"When the voltage of this pin falls below the enable threshold for more than 10ms, the IC turns off."
I think that TPS61500 is operated at the moment(about 10ms) even if EN is asserted Low due to this.
Is my understanding correct ?
Is my understanding correct ?
Best Regards,
Ryuji Asaka