Other Parts Discussed in Thread: BQ34Z100
Hello,
we are designing a multicell, Li-ion battery pack with bq34z100-based gas gauging. We need the charging voltage (thus the resulting capacity) to be variable, that is, before initiating every charge, the applied charging voltage is chosen. For example, choosing a 4.1V per cell instead of 4.2V would result in a final remaining capacity of, say, 90% instead of 100%.
I was trying to understand if this could be a problem for the gas gauging algorithms and for their accuracy and if we need to reconfigure from time to time some parameters (e.g. Charging Voltage).
Thanks,
DZ