Other Parts Discussed in Thread: TPS92075
The TPS92075 datasheet includes a current limit voltage 1.2V on ISNS. Would this cause an overstress of the switching MosFET and recirc diode (reset delay 280us) switching at a lower freq?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS92075
The TPS92075 datasheet includes a current limit voltage 1.2V on ISNS. Would this cause an overstress of the switching MosFET and recirc diode (reset delay 280us) switching at a lower freq?
Thanks.
Hi,
Voltage Vcl=1.2V determine the current level when control logic switch off the switching MOSFET. Taking into account that operated voltage at ISNS =0.5V, this mean that current limit feature turn on when current increase more than 2x. This shouldn't overstress MOSFET if it was right selected.
The 1.2V current limit threshold, if reached, will cause switching to stop and a 280us delay to occur before switching begins again. This feature is really meant to help in cases where there is a very hard short circuit - like output inductor shorted, for example. Otherwise the 1.2V level is not likely to be reached because the regular operation of the deivce will already have shut the FET off before this level. For example, in normal operation the parallel comparator will reach its threshold first at a level of 1V max, it takes a very low impedance short to have the current reach the 1.2V level, but in case it does, the longer restart will help save the device.