Hi guys,
I actually have problems designing a charger detection for the bq77908a. The one I built is sending out a pulse to CHGST every time the Pack(-) terminal gets defined. Problem thereby is that I run the system in series FET configuration for lower space consumption and need to pull down CPCKN when the system goes in shutdown mode (datasheet page 32). This pulldown defines my Pack(-) terminal again and lets my charger detection wake the chip up again. Consequently it's swinging on and off all the time when it should be in shutdown mode.
Now I have 2 pleases to you. First one is to explain me detailed what DPCKN and CPCKN do and how they work, because it's very confusing to me what's written down in the datasheet about them. All I know so far is that these pins have something to do with the load detection. My first idea to solve the problem above was to put a diode between CPCKN and the Pack(-) terminal for releasing the Pack(-) terminal from the pulldown, but I think this would have influence on some chip safety functions, right?
The second one is to tell me how I can use the CPCKN pin for charger detection as offered on page 9 of the datasheet.
I really appreciate your help!
Best Regards,
Konstantin Nickel