This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ryuji,
All existing LP8556 device options are optimized for 25 mA/CH or less. While you may use the RISET to adjust the current up or down from the nominal ILED of 23mA for the LP8558-E08, the Vheadroom settings can only support up to 25mA/CH. Supporting 50 mA/CH requires optimazing the DRIVER_HEADROOM (register AAh) and HEADROOM_OFFSET (register 9Eh) settings. Overriding the existing settings (or EPROM defaults) requires system's ability to send I2C commands. If the I2C is not available in the system, a new device option may be requested.
Regards,
Davor