This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51206 VDDQSNS and VTT/VTTREG operating range

Other Parts Discussed in Thread: TPS51206

The TPS51206 datasheet says VDDQSNS max is 3.5V. However, its first page also states VTT output range is 0.5V to 0.9V for DDR applications with VDDQ at 1.8V, 1.5V, 1.35V, etc.

Can the TPS51206 be used reliably to track a VDDQSNS voltage level higher than 1.8V, such as 3.3V, to get half of the voltage level at VDDQSNS for VTT/VTTREF such as 1.65V (higher than the stated 0.9V)? 

Thanks!