This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Regarding to select Li-Polymer Battery charger IC and energy Indicator IC

Dear TI,

1. Presently we are using TPS62090 regulator for our device. But now we need to change the regulator because we need to utilize the full battery voltage level even if reach till 3V. So we are choosing TPS63001 (If not, advice better one).

Device Requirement:

3.3V,1.2A

2. We need Battery charger IC,So please suggest the suitable IC for our requirement.

Requirement:

Li-Polymer Battery(2cells in parallel) 3.7V,20Ah.

Charging voltage for battery 4.2V,4Ah

input voltage for charger IC 5V

3. We need to display the remaining capacity of the battery like all mobiles do.And also we need to measure and display the battery temperature.So please suggest me the suitable IC(fuel gauge /gas gauge/energy indicator) for this application.

We are waiting for your response.

Regards,

Naveen K