Hello,
Our customer has the following question:
"I was looking at the 32.768KHz clock generation circuit on the TPS65930 and noticed in the data manual (page 83) that an external crystal can only be used in master mode; in slave mode the TRM (page 100) says that the internal oscillator circuitry is bypassed and it requires an external signal to be applied.
Is that correct - if I configure the device in slave mode I have to use an external oscillator instead of just a crystal?
If so, why would that be?
On our prototype board I will have options to boot in either mode, but our production design would not use a power-on button and
so I was planning to use slave mode and kick it off with the 3.3V PG signal. "
Please comment on question.
Thanks.