This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Wide input range Isolated DC-DC convertor



Hi,

I need to design an isolated DCDC convertor with input range of 6-110V and output voltage of 12 @ 0.2A. 

I've used Webench and didnt really get anywhere. I could probably settle to split the input voltage range into two overlapping ranges, so long as tehy are using the same IC and its a case of swapping a resistor value.

Was anyone aware of an IC that would help in this design?

Thanks,