Dear all,
we have problem with TPS61020 chip. We made 150pcs products with this IC and about 30pcs have problem with powering after few months. In normal state, there is 3,15V output voltage and about 45mA of output power when active and 50uA when standby mode. On defective units is right voltage, but current about 50-150mA in standby mode and 150-250mA in active mode. When we change this IC, there are right currents, so it has to be TPS61020 problem. We are desperate.. All products have the same PCB, same values of components. Same reflow, etc. We thought it could be ESD problem. Any ideas? Thank you very very much! Jan Zastera
Schematic is here: http://www.janzaudio.com/upload/scheme.png
(FPC5 is an input/output connector of signal)