This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ20z95 replace with BQ20z65

Other Parts Discussed in Thread: BQ20Z655-R1

Hello,

I am using BQ20z95 in a large scale and at this point it is not possible for me to go to another Circuit.So i need a favor from you.

I need a Crystal Segment Display   in Place of LED Display i know that BQ20z95 Doesn't support the LCD Display.

And your Ic BQ20z655 supports the Crystal Segment Display . if in my Circuit I replace the BQ20z95 with BQ20z655 will it work .Because the Pin Configuration of both are same the only difference  in it is its  Led OUT pin(8) i.e One Cap. n resistor is connected and also the Common of LCD is Connected to nc pin (12)

if i make the same difference in my circuit  and replace the Ic will it work or no.

Please Reply ASAP as it is urgent project

Regards

Tanvi