Hi.
I have a problem to found the exactly value of the operation frequency in my application. I didn't find any informations to how can I calculate the operating frequency on my case specifically.
I'm using the following parameters.
NCell = 8 Mi-MH
Vin[MAX] = 36V
Vout= 8 * 1,7 = 13,6
Rsns = 0,056Ohms
Chys = 4,7pF
Ic =0,9A(Charge Current)
So, the ApplicationNote says:
"The six values that determine operating frequency are input voltage VIN, inductance L, sense resistor RSNS, filter resistance RF, filter capacitance CF, and hysteresis capacitor CHYS."
and
"Select the desired maximum operating frequency F.This is the frequency of operation when the output voltage is exactly half the input voltage. At duty cycles of 75% or 25%, the frequency is 75% of this value."
Is this the best method to find the maximum operating frequency? Does exist any other form to calculate the operating frequency of the specific circuit?