Other Parts Discussed in Thread: TPS2359, TPS2459
Hello, My application requirements are the following
- Two OR-ed channels, current drawn from both
- Ability to control the current contribution from each channel. For example, 40% current from channel1 and 60% from channel2
- Ability to dynamically change the current contribution from each channel, through a i2c interface
After searching for parts, I could find TPS2359 and TPS2459 that match my requirements. Is my finding correct?
For the above requirements, do both TPS2359 & 2459 satisfy the requirements? Is there any difference between the two that will make one of them better for my application?
Thanks
David