Hi,
I am using the TPS61092 in a simple boost application (see attached schematic) but when I power the system and vary the input voltage from 1.9V to 5V the output tracks along with it (it has about a 300mV offset, Vin = 1.9V Vout = 2.2V) till Vin reaches 4.3V and then the output jumps to 5V. The circuit seems simple enough and I am sure I am missing something